Real Time

Configure PUSCH Auto-calculate

PUSCH Auto-calculate per-slot params 

Choice: Off | On

Default Off

Double-click or use the drop-down menu to turn automatic calculation of per-slot parameters on or off.

To enable manual input for the following parameters, set PUSCH Auto-calculate per-slot params to Off:

DMRS Sequence Index for slot 0/1, DMRS Group Index for slot 0/1, and DMRS Cyclic Shift for slot 0/1 in the Physical Channel node.

To enable manual input for the following parameters, set PUSCH Auto-calculate per-slot params to On:

PUSCH nDMRS(1), PUSCH nDMRS(2), PUSCH Delta SS (described below)

Hopping in the Cell Parameters section of the Uplink node.

PUSCH nDMRS(1)

Range: 0 to (Maximum resource elements – 1)

Default: 0

When PUSCH Auto-calculate per-slot params is turned On, you can enter a value for PUSCH nDMRS(1). This value is used to calculate the Cyclic Shift Alpha (see 3GPP TS36.211).

PUSCH nDMRS(2)

Choice: 0 | 2 | 3 | 4 | 6 | 8 | 9 | 10

Default: 0

When PUSCH Auto-calculate per-slot params is turned On, double-click or use the drop-down menu to select a value for PUSCH nDMRS(2). This value is used to calculate the Cyclic Shift Alpha (see 3GPP TS36.211).

PUSCH Delta SS

Range: 0 to 29

Default: 0

When PUSCH Auto-calculate per-slot params is turned On, you can enter a value for PUSCH Delta SS. This value is used to calculate the sequence-shift pattern (see 3GPP TS36.211).

PUSCH Frequency Hopping

Choice: Off | On

Default Off

Double-click or use the drop-down menu to turn PUSCH frequency hopping on or off.

PUSCH Frequency Hopping Mode

Displays the PUSCH frequency hopping mode (see 3GPP TS36.211).

PUSCH Frequency Hopping Type

Displays the PUSCH frequency hopping type (see 3GPP TS36.211).

PUSCH Hopping Offset (N_HO_RB)

Displays the PUSCH Frequency Hopping Offset value (see 3GPP TS36.211).

Number of Sub-bands (Nsb)

Displays the number of sub-bands (Nsb) (see 3GPP TS36.211).

CURRENT_TX_NB mod 2

Displays the value for CURRENT_TX_NB mod 2 (see 3GPP TS36.211).